SLUSD66D September 2019 – February 2021 TPS92520-Q1
PRODUCTION DATA
The write response frame has the following format:
Figure 7-18 shows the write response format. This frame is sent out following a write command if the previously received frame was a write command and no SPI error occurred during that frame.
The data bits in the write response are read back from the destination register that was just written. There is no need to issue a read command and evaluate the read response in order to check that the destination register was written correctly.