SLVSEC4B April 2019 – January 2020 TPS92613-Q1
PRODUCTION DATA.
The TPS92613-Q1 device is a high-side current driver for driving LEDs. The device controls the output current through regulating the voltage drop on an external high-side current-sense resistor, R(SNS). An integrated error amplifier drives an internal power transistor to maintain the voltage drop on the current-sense resistor R(SNS) to V(CS_REG) and therefore regulates the current output to target value. When the output current is in regulation, the current value can be calculated by using Equation 1.
where
When the supply voltage drops below total LED string forward voltage plus required dropout voltage, V(DROPOUT), the TPS92613-Q1 is not able to deliver enough current output as set by the value of R(SNS), and the voltage across the current-sense resistor R(SNS) is less than V(CS_REG).