SLVSHB8 august 2023 TPS92621-Q1
PRODUCTION DATA
The TPS92621-Q1 device consumes minimal quiescent current, I(FAULT), into SUPPLY when the FAULT pin is externally pulled LOW. At the same time, the device shuts down the output.
If device detects an internal fault, it pulls down the FAULT pin by an internal typical 3-mA constant current as a fault indication to the fault bus.