SLUSCX8C March 2019 – March 2021 TPS92682-Q1
PRODUCTION DATA
If CHxOVEN is set to "1" in the FEN1 Register, the output over voltage fault is enabled. When VFBx exceeds the threshold voltage OVTHR, the CHx_OV fault is set high and turns off the associated channel. The OVTHR voltage is set by OV_DAC; OVTHR = VFBREF × OV%, where OV% is provided in the OV Register. The VFBREF in CC mode is set to 1.228 V (typical), and in CV mode, is set to the output of the CHxIADJ register. When CHx_OV is high, OVTHR is set to VFBREF and a 20 µA hysteresis current is applied to the feedback resistor divider. For the boost converter with the output voltage sensing according to Figure 7-15, VOUT must decrease to a level shown in Equation 6 for the CHx_OV to be cleared.
If the CHxOVFL bit is set to "1" in the FLATEN Register, the OV fault is configured as a latched fault and the associated channel turns off with the rising edge of CHx_OV. The channel can be turned on again only by re-setting the CHxEN bit in the EN Register.
For CHxOVFL = 0, the OV fault is a non-latched fault. In this case, the associated channel turns off when the OV fault occurs, but the channel goes through a restart and soft-start ramp when CHx_OV goes low. Figure 7-16 shows a non-latched OV situation for a converter in CV mode, where the output voltage (VFBx) is regulated to VFBREF in normal condition.