SNVSC83B September 2022 – February 2023 TPSM365R3 , TPSM365R6
PRODUCTION DATA
Voltage at the EN pin controls the start-up or remote shutdown of the TPSM365Rx. The part stays shut down as long as the EN pin voltage is less than VEN-WAKE = 0.4 V. During the shutdown, the input current drawn by the device typically drops down to 0.5 µA (VIN = 13.5 V). With the voltage at the EN pin greater than VEN-WAKE, the device enters device standby mode and the internal LDO powers up to generate VCC. As the EN voltage increases further, approaching VEN-VOUT, the device finally starts to switch, entering start-up mode with a soft start. During the device shutdown process, when the EN input voltage measures less than (VEN-VOUT–VEN-HYST), the regulator stops switching and re-enters device standby mode. Any further decrease in the EN pin voltage, below VEN-WAKE, and the device is then firmly shut down. The high-voltage compliant EN input pin can be connected directly to the VIN input pin if remote precision control is not needed. The EN input pin must not be allowed to float.
The various EN threshold parameters and their values are listed in the GUID-XXXXXXXX-SF0T-XXXX-XXXX-000000280921.html#GUID-XXXXXXXX-SF0T-XXXX-XXXX-000000280921. #T5988933-33 shows the precision enable behavior and #T5988933-14 shows a typical remote EN start-up waveform in an application. After EN goes high, after a delay of about 1 ms, the output voltage begins to rise with a soft start and reaches close to the final value in about 2.58 ms (tss). After a delay of about 1.956 ms (tPGOOD_ACT), the PG flag goes high. During start-up, the device is not allowed to enter FPWM mode until the soft-start time has elapsed. This time is measured from the rising edge of EN.
External UVLO via EN pin
In some cases, an input UVLO level different than that provided internal to the device is needed. This can be accomplished by using the circuit shown in #SNVSAW13754. The input voltage at which the device turns on is designated as VON while the turn-off voltage is VOFF. First, a value for RENB is chosen in the range of 10 kΩ to 100 kΩ, then #GUID-A9D0E03A-6980-4EBD-B6BB-1A96AA10652E and #GUID-8387CD61-5E27-4D9F-9923-17AF8BCA2487 are used to calculate RENT and VOFF, respectively.
where