SCDS364E June 2015 – October 2019 TS5A22362
PRODUCTION DATA.
Ensure that the device is powered up with a supply voltage on VCC before a voltage can be applied to the signal paths NC and NO.
Tie the digitally controlled inputs select pins IN1 and IN2 to VCC or GND to avoid unwanted switch states that could result if the logic control pins are left floating.
All unused digital inputs of the device must be held at VCC or GND to ensure proper device operation. Refer to the TI application report, Implications of Slow or Floating CMOS Inputs, SCBA004.