SLLSEN9F May 2015 – March 2022 TUSB320
PRODUCTION DATA
During dead battery mode, VDD is not available. CC pins always default to pulldown resistors in dead battery mode. Dead battery mode means:
Upon exiting dead battery mode (VDD is active), the software must perform the following sequence in order for Rp to be presented on both CC pins:
Between steps 1 and 3, the status flags will be set. The software must ignore these flags when performing the three steps.
When VDD is off, the TUSB320 non-failsafe pins ( VBUS_DET, ADDR, PORT, ID, OUT[3:1] pins) could back-drive the TUSB320 device if not handled properly. When necessary to pull these pins up, it is recommended to pullup PORT, ADDR, INT_N/OUT3, and ID to the device’s VDD supply. The VBUS_DET must be pulled up to VBUS through a 900-kΩ resistor.