SLLSEF7 March 2014 TUSB8020B-Q1
PRODUCTION DATA.
The TUSB8020B-Q1 is a two-port USB 3.0 compliant hub. It provides simultaneous SuperSpeed USB and high-speed/full-speed connections on the upstream port and provides SuperSpeed USB, high-speed, full-speed, or low speed connections on the downstream port. The TUSB8020B-Q1 can be used in any application that needs additional USB compliant ports. For example, a specific notebook may only have two downstream USB ports. By using the TUSB8020B-Q1, the notebook can increase the downstream port count to three.
A common application for the TUSB8020B-Q1 is as a self powered standalone USB hub product. The product is powered by an external 5V DC Power adapter. In this application, using a USB cable TUSB8020B-Q1’s upstream port is plugged into a USB Host controller. The downstream ports of the TUSB8020B-Q1 are exposed to users for connecting USB hard drives, camera, flash drive, and so forth.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
VDD Supply | 1.1V |
VDD33 Supply | 3.3V |
Upstream Port USB Support (SS, HS, FS) | SS, HS, FS |
Downstream Port 1 USB Support (SS, HS, FS, LS) | SS, HS, FS, LS |
Downstream Port 2 USB Support (SS, HS, FS, LS) | SS, HS, FS, LS |
# of Removable Downstream Ports | 2 |
# of Non-Removable Downstream Ports | 0 |
Full Power Management of Downstream Ports | Yes. (FULLPWRMGMTZ = 0) |
Individual Control of Downstream Port Power Switch | Yes. (GANGED = 0) |
Power Switch Enable Polarity | Active High. (PWRCTL_POL = 0) |
Battery Charge Support for Downstream Port 1 | Yes |
Battery Charge Support for Downstream Port 2 | Yes |
I2C EEPROM Support | No. |
24MHz Clock Source | Crystal |
The upstream of the TUSB8020B-Q1 is connected to a USB3 Type B connector. This particular example has GANGED terminal and FULLPWRMGMTZ terminal pulled low which results in individual power support each downstream port. The VBUS signal from the USB3 Type B connector is feed through a voltage divider. The purpose of the voltage divider is to make sure the level meets USB_VBUS input requirements.
The downstream port 1 of the TUSB8020B-Q1 is connected to a USB3 Type A connector. With BATEN1 terminal pulled up, Battery Charge support is enabled for Port 1. If Battery Charge support is not needed, then pull-up resistor on BATEN1 should be uninstalled. The PWRCTL_POL is pulled down which will result in active high power enable (PWRCTL1 and PWRCTL2) for a USB VBUS power switch.
The downstream port 2 of the TUSB8020B-Q1 is connected to a USB3 Type A connector. With BATEN2 terminal pulled up, Battery Charge support is enabled for Port 2. If Battery Charge support is not needed, then pull-up resistor on BATEN2 should be uninstalled.
This particular example uses the Texas Instruments TPS2561 dual channel precision adjustable current-limited power switch. For details on this power switch or other power switches available from Texas Instruments, please refer to the Texas Instruments website.