One must pay close attention to PCB layout in
order to achieve optimum performance for the UCC21551x-Q1. Below
are some key points.
Component Placement:
- Low-ESR and low-ESL capacitors must be connected close to the device between the VCCI and GND pins and between the VDD and VSS pins to support high peak currents when turning on the external power transistor.
- To avoid large negative transients on the switch node VSSA (HS) pin, the parasitic inductances between the source of the top transistor and the source of the bottom transistor must be minimized.
- It is recommended to place the dead-time setting resistor, RDT, and
its bypassing capacitor close to DT pin of the UCC21551x-Q1.
- It is recommended to bypass using a ≈1nF low
ESR/ESL capacitor, CEN, close to EN pin when connecting to a µC with
distance.
Grounding Considerations:
- It is essential to confine the high peak currents that charge and discharge the transistor gates to a minimal physical area. This will decrease the loop inductance and minimize noise on the gate terminals of the transistors. The gate driver must be placed as close as possible to the transistors.
- Pay attention to high current path that includes the bootstrap capacitor, bootstrap diode, local VSSB-referenced bypass capacitor, and the low-side transistor body/anti-parallel diode. The bootstrap capacitor is recharged on a cycle-by-cycle basis through the bootstrap diode by the VDD bypass capacitor. This recharging occurs in a short time interval and involves a high peak current. Minimizing this loop length and area on the circuit board is important for ensuring reliable operation.
High-Voltage Considerations:
- To ensure isolation performance between the
primary and secondary side, one should avoid placing any PCB traces or copper
below the driver device. A PCB cutout is recommended in order to prevent
contamination that may compromise the UCC21551x-Q1’s
isolation performance.
- For half-bridge, or high-side/low-side configurations, where the channel A and channel B drivers could operate with a DC-link voltage up to 1500 VDC, one should try to increase the creepage distance of the PCB layout between the high and low-side PCB traces.
Thermal Considerations:
- A large amount of power may be dissipated by the
UCC21551x-Q1 if
the driving voltage is high, the load is heavy, or the switching frequency is
high (refer to Section 8.2.2.5 for more details). Proper PCB layout can help dissipate heat from the device
to the PCB and minimize junction to board thermal impedance
(θJB).
- Increasing the PCB copper connecting to VDDA, VDDB, VSSA and VSSB pins is recommended, with priority on maximizing the connection to VSSA and VSSB (see Figure 10-2 and Figure 10-3). However, high voltage PCB considerations mentioned above must be maintained.
- If there are multiple layers in the system, it is also recommended to connect the VDDA, VDDB, VSSA and VSSB pins to internal ground or power planes through multiple vias of adequate size. However, keep in mind that there shouldn’t be any traces/coppers from different high voltage planes overlapping.