SLUSD05B October 2017 – August 2018 UCC27710
PRODUCTION DATA.
The UCC27710 device output stage pull-up structure features a P-Channel MOSFET to provide source current until the output is saturated to VDD or HB. The ROH parameter (see Figure 21 ) is a DC measurement and it is representative of the on-resistance of the P-Channel device.
The pull-down structure in UCC27710 is composed of a N-Channel MOSFET. The ROL parameter (see Figure 19) , which is also a DC measurement, is representative of the impedance of the pull-down stage in the device.
Each output stage in UCC27710 is capable of supplying 0.5-A peak source and 1.0-A peak sink current pulses. The output voltage swings between (VDD and COM) / (HB and HS) providing rail-to-rail operation, thanks to the MOSFET output stage which delivers very low drop-out.