SLUS495J August 2001 – December 2023 UCC29002 , UCC39002
PRODUCTION DATA
The UCC29002 device operates in this mode when the current-sense amplifier inputs are biased as described in the Enable Function (CS+, CS–) section, or when the VDD voltage is below the start-up threshold as described in the Bias and Bias OK Circuit (VDD) section, or when a bus-fault condition has been detected as described in the Fault Protection on LS Bus section.
In this mode, the UCC29002 device CSO output is disconnected from the LS Bus and the Adjust amplifier input is grounded to set the ADJ current to zero.