SLUSFF2 October 2024 UCG28826
ADVANCE INFORMATION
The high voltage (HV) pin should be connected to the two ends of the X-capacitor at the line input, through two diodes as shown in Figure 6-1. This pin charges the bias supply (VCC) capacitor at startup. The HV pin also discharges the X-capacitor when the input line voltage is removed.