SBOS913 February 2018 XTR305
PRODUCTION DATA.
It is possible to drive the XTR305 with a unidirectional input signal and still get a bidirectional output by adding an additional resistor, ROS, and an offset voltage signal, VREF. It can be a mid-point voltage or a signal to shift the output voltage to a desired value.
This design is illustrated in Figure 43a, Figure 43b, and Figure 43c. As with a normal operational amplifier, there are several options for offset-shift circuits. The input can be connected for inverting or noninverting gain. Unlike many op amp input circuits, however, this configuration uses current feedback, which removes the voltage relationship between the noninverting input and output potential because there is no feedback resistor.
The input bias current effect on the offset voltage can be reduced by connecting a resistor in series with the positive input that matches the approximate resistance at the negative input. This resistor placed close to the input pin acts as a damping element and makes the design less sensitive to RF noise. See R3 in Figure 40.