The device requires two different
power-supply voltages. 1.9-V DC is required for the VA19 power bus and 1.1-V DC is
required for the VA11 and VD11 power buses. The power-supply voltages must be low
noise and provide the needed current to achieve rated device performance. There are
two recommended power supply architectures:
- Step down using high-efficiency switching converters, followed
by a second stage of regulation to provide switching noise reduction and
improved voltage accuracy.
- Directly step down the final ADC supply voltage using
high-efficiency switching converters. This approach provides the best
efficiency, but care must be taken for switching noise to be minimized to
prevent degraded ADC performance. This approach is best described in the
following application note: Powering Sensitive ADC Designs with the
TPS62913 Low-Ripple and Low-Noise Buck Converter.
TI WEBENCH® Power Designer can be used to select and design the individual
power supply elements needed: see the WEBENCH® Power Designer
- Decouple all power supply rails
and bus voltages as they come onto the system board and near/at the ADC itself.
Typically, one decoupling capacitor per power supply pin is sufficent unless
specified in the datasheet or EVM assembly.
- Remember that approximately 20
dB/decade noise suppression is gained for each additional filtering stage.
- Decouple for both high and low
frequencies, which might require multiple capacitor values.
- Series ferrite beads are commonly
used at the power plain entry point. This should be done for each individual
supply voltage on the system board whether it comes from an LDO or a switching
regulator.
- For added capacitance, use
tightly stacked power and ground plane pairs (≤4 mil spacing) this adds inherent
high-frequency (>500MHz) decoupling to the PCB design.
- Keep supplies away from sensitive
analog circuitry such as the front-end RF stage of the ADC and high-speed
clocking & digital circuits if possible.
- Some switcher regulator
circuitry/components could be located on the opposite side of the PCB for added
isolation.
- Follow the IC manufacture
recommendations; if they are not directly stated in the application note or data
sheet, then study the evaluation board. These are great vehicles to learn from.
Applying these points above can help provide a solid power supply design
yielding datasheet performance in many applications.
Each application will have different
tolerances for noise on the supply voltage so understanding these trades is best
described in the following two application notes for more details:
- Clutter-free power supplies for RF converters
in radar applications (Part 1)
- Clutter-free power supplies for RF converters
in radar applications (Part 2)
Also refer to both Figure 8-5 and Figure 8-6 to illustrate a
few different approaches.