JAJSP68 August 2022 ADC3564
PRODUCTION DATA
The ADC3564 includes a MUX in front of the digital decimation filter which allows the ADC to be connected to two digital down converters (see Figure 8-14). This enables dual band complex decimation. The NCO of each digital down converter can be tuned to an independent frequency across the Nyquist zone as illustrated in the example in Figure 8-15. The second DDC is output using the DB0/1 SLVDS interface.