The device includes a mode where the contents of the internal registers can be read back using the SDIO pin. This readback mode can be useful as a diagnostic check to verify the serial interface communication between the external controller and the ADC. The procedure to read the contents of the serial registers is as follows:
Drive the SEN pin low
Set the R/W bit (A15) to 1. This setting disables any further writes to the registers. Set A[14:12] in address field to 0.
Initiate a serial interface cycle specifying the address of the register (A[11:0]) whose content must be read
The device launches the contents (D[7:0]) of the selected
register on the SDIO pin on SCLK falling edge
The external controller can capture the contents on the
SCLK rising edge