Employ best design practices when laying out a
printed circuit board (PCB) for both analog and digital components. For optimal
performance, separate the analog components [such as ADCs, amplifiers, references,
digital-to-analog converters (DACs), and analog MUXs] from digital components [such
as microcontrollers, complex programmable logic devices (CPLDs), field-programmable
gate arrays (FPGAs), radio frequency (RF) transceivers, universal serial bus (USB)
transceivers, and switching regulators]. Figure 9-12 shows an example of good component placement. Although Figure 9-12 provides a good example of component placement, the best placement for each
application is unique to the geometries, components, and PCB fabrication
capabilities employed. That is, there is no single layout that is perfect for every
design and careful consideration must always be used when designing with any analog
component.
The following outlines some basic recommendations for the layout of the ADS101xL to get the best possible performance of the ADC. A good design can be ruined with a bad circuit layout.
- Separate analog and digital signals. To start,
partition the board into analog and digital
sections where the layout permits. Route digital
lines away from analog lines. This placement
prevents digital noise from coupling back into
analog signals.
- Fill void areas on signal layers with ground fill.
- Provide good ground return paths. Signal return
currents flow on the path of least impedance. If
the ground plane is cut or has other traces that
block the current from flowing right next to the
signal trace, the current must find another path
to return to the source and complete the circuit.
A longer return current path increases the chance
that the signal radiates. Sensitive signals are
more susceptible to EMI interference.
- Use bypass capacitors on supplies to reduce
high-frequency noise. Do not place vias between bypass capacitors and the
active device. Placing the bypass capacitors on the same layer as close to
the active device yields the best results.
- Consider the resistance and inductance of the
routing. Often, traces for the inputs have resistances that react with the
input bias current and cause an added error voltage. Reduce the loop area
enclosed by the source signal and the return current to reduce the
inductance in the path. Reduce the inductance to reduce the EMI pickup, and
reduce the high-frequency impedance observed by the device.
- Differential inputs must be matched for both the inputs going to the measurement source.
- Analog inputs with differential connections must
have a capacitor placed differentially across the inputs. Best input
combinations for differential measurements use adjacent analog input lines
(such as AIN0, AIN1 and AIN2, AIN3). The differential capacitors must be of
high quality. The best ceramic chip capacitors are C0G (NPO), which have
stable properties and low-noise characteristics.