JAJSL30 July 2023 ADS131B24-Q1
PRODUCTION DATA
The UNLOCK command unlocks the interface if previously locked by the LOCK command.
The LOCK status bit and the command response in the next frame indicate if the UNLOCK command executed successfully or if an error occurred that prevented the UNLOCK command from executing. A NULL command is executed if the UNLOCK command did not execute.
Figure 9-34 shows an UNLOCK command frame where no faults occurred during the communication.