JAJSFC6C May 2015 – April 2018 ADS52J90
PRODUCTION DATA.
The device JESD204B transmitter uses differential CML output drivers with a typical current drive of 16 mA. The output driver includes an internal 50-Ω termination to the DVDD_1P2 supply. Additionally, external 50-Ω termination resistors connected to DVDD_1P2 must be placed close to the receiver pins. DC compliance to the standard is not ensured and ac coupling can be used to avoid the common-mode mismatch between the transmitter and receiver, as shown in Figure 77.
The CML buffer also has a pre-emphasis control for improving the timing margins. Pre-emphasis is achieved by increasing the CML buffer current if the current transmitter bit is different from the previous one. The current of the CML buffer for a transitioning bit can be increased from the CML buffer current setting to one of 16 settings in steps of 0.25 mA using the PRE_EMP register control. Pre-emphasis is recommended to be used at higher speeds in order to improve the timing margins.