JAJSVV8 December 2024 AFE5401-EP
PRODUCTION DATA
In this mode, the DECIMATE_2_EN, DECIMATE_4_EN, and FILT_EN register bits must be set, and the filter coefficients should be configured. Figure 5-1 shows a typical filter response in decimate-by-4 mode for the filter coefficient of set 1 (default) and set 2. Note that the output data rate is reduced by a factor of 4 as compared to default mode for the given clock input frequency.