SBASB81 December 2024 AFE5401-EP
PRODUCTION DATA
In some applications, the input signal power linearly decreases with signal frequency. Such types of input spectrum can be equalized using a first-order signal equalizer. The device can be configured in two different equalizer modes: EQ_EN and EQ_EN_LOW_FC. Table 7-11 lists the register settings for these modes.
EQ_EN | EQ_EN_LOW_FC | DESCRIPTION |
---|---|---|
0 | 0 | Default mode |
0 | 1 | Default mode |
1 | 0 | Equalizer enabled |
1 | 1 | Equalizer with low-corner frequency enabled |
The HPF and LPF cutoff frequencies (of the antialiasing filter) are the same as per the FILTER_BW setting. In this mode, overall channel gain increases by an additional fixed gain of 15 dB from the HPF block. Typical frequency response plots showing different equalizer modes along with the default mode are shown in Figure 7-9 and Figure 7-10.