JAJSPQ1 August 2024 AMC0106M05
ADVANCE INFORMATION
In Figure 7-1, the high-side power supply (AVDD) is generated from a bootstrap circuit (R4, D1, C2).
The high-side ground reference (AGND) is derived from the end of the shunt resistor connected to the negative input of the AMC0106M05 (INN). For a four-terminal shunt, connect the device inputs to the inner leads of the shunt and connect AGND to the outer leads. To minimize offset and improve accuracy, route the ground connection as a separate trace. Connect AGND directly to the shunt resistor rather than shorting AGND to INN at the input to the device. See the Layout section for more details.