JAJSRV8A August 2024 – December 2024 AMC0136
PRODUCTION DATA
Do not leave the analog input (INP pin) of the AMC0136 unconnected when the device is powered up. If the device input is left floating, the output of the device is not valid.
Do not connect protection diodes to the input (INP pin) of the AMC0136. Diode leakage current potentially introduces significant measurement error especially at high temperatures. The input pin is protected against high voltages by the ESD protection circuit and the high impedance of the external resistive divider.