JAJS323D February 2008 – June 2024 AMC1203
PRODUCTION DATA
Place a minimum 10nF capacitor at the input of the device (from INP to INN). This capacitor helps avoid voltage droop at the input during the sampling period of the switched-capacitor input stage.
Do not leave the inputs of the AMC1203 unconnected (floating) when the device is powered up. If the device inputs are left floating, the input bias current potentially drives the inputs to a positive value exceeding the operating common-mode input voltage. As a result, DOUT is permanently high.
Connect the high-side ground (AGND) to INN, either by a hard short (at the shunt, not at the device pins) or through a resistive path. A DC current path between INN and AGND is required to define the input common-mode voltage. Take care not to exceed the input common-mode range as specified in the Recommended Operating Conditions table. For best accuracy, route the ground connection as a separate trace to the shunt. See the Layout section for more details.