JAJSHC4A May 2019 – November 2019 ATL431LI-Q1 , ATL432LI-Q1
PRODUCTION DATA.
Though ATL431LI-Q1 is stable with no capacitive load, the device that receives the output voltage of the shunt regulator can present a capacitive load that is within the ATL431LI-Q1 region of stability, shown in Figure 13. Also, designers can use capacitive loads to improve the transient response or for power supply decoupling. When using additional capacitance between Cathode and Anode, see Figure 13. Also, Understanding Stability Boundary Conditions Charts in TL431, TL432 Data Sheet Application Note provides a deeper understanding of the stability characteristics of this device and aids the user in making the right choices when choosing a load capacitor.