JAJSPK3G May 2001 – December 2022 BQ2057C
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The BQ2057 is designed to work with both PNP transistor and P-channel MOSFET. The device should be chosen to handle the required power dissipation, given the circuit parameters, PCB layout and heat sink configuration. The following examples illustrate the design process for either device:
PNP transistor: Selection steps for a PNP bipolar transistor: Example: VI = 4.5 V, I(REG) = 1 A, 4.2-V single-cell Li-Ion (bq2057C). VI is the input voltage to the charger and I(REG) is the desired charge current (see Figure 10-1).
Now choose a device package with a theta at least 10% below this value to account for additional thetas other than the device. A SOT223 package, for instance, has typically a theta of 60°C/W.
where Imax(C) is the maximum collector current (in this case same as I(REG)), and IB is the base current (chosen to be 35 mA in this example).
The beta of a transistor drops off by a factor of 3 over temperature and also drops off with load. Therefore, note the beta of device at I(REG) and the minimum ambient temperature when choosing the device. This beta should be larger than the minimum required beta.
Now choose a PNP transistor that is rated for V(CE) ≥15 V, θJC ≤ 78°C/W, IC ≥ 1.5 A, βmin ≥ 28 and that is in a SOT223 package.
P-channel MOSFET: Selection steps for a P-channel MOSFET: Example: VI = 5.5 V, I(REG) = 500 mA, 4.2-V single-cell Li-Ion (BQ2057C). VI is the input voltage to the charger and I(REG) is the desired charge current. (See Figure 10-4.)
Now choose a device package with a theta at least 10% below this value to account for additional thetas other than the device. A TSSOP-8 package, for instance, has typically a theta of 70°C/W.
Where V(GS) is the gate-to-source voltage, VD is the forward voltage drop across the reverse-blocking diode (if one is used), and VCS is the voltage drop across the current sense resistor, and VOL(CC) is the CC pin output low voltage specification for the BQ2057.
Select a MOSFET with gate threshold voltage, V(GSth), rating less than the calculated V(GS).
Now choose a P-channel MOSFET transistor that is rated for VDS ≤ −15 V, θJC ≤ 110°C/W, ID ≥ 1 A, V(GSth) ≥ −3.5 V and in a TSSOP package.