JAJSPL3 January 2023 BQ21080
PRODUCTION DATA
There are two programmable wake or short button press timers, WAKE1 and WAKE2. There are no specific actions taken by the tWAKE1 or tWAKE2 durations other than issuing an interrupt and updating the wake registers. For a wake from shipmode event when the button press is enabled, the push button has to be low for tshipwake before the device can turn ON the SYS rail.
In the case where a valid VIN (VIN > VUVLO) is connected prior to the tshipwake timer expiring, the device will exit shipmode immediately regardless of the TS/MR or wake timer state. Refer to GUID-71AA00C0-FA07-42CB-AFA5-8E32EDD44CC6.html for more details.