JAJSL87H january 2010 – april 2021 BQ24090 , BQ24091 , BQ24092 , BQ24093 , BQ24095
PRODUCTION DATA
The battery detect routine should check for a missing battery while keeping the OUT pin at a useable voltage. Whenever the battery is missing the CHG pin should be high impedance.
The battery detect routine is run when entering and exiting TTDM to verify if battery is present, or run all the time if the battery is missing and not in TTDM. On power up, if battery voltage is greater than VRCH threshold, a battery detect routine is run to determine if a battery is present.
The battery detect routine is disabled while the IC is in TTDM or has a TS fault. See Figure 9-7 for the battery detect flow diagram.