JAJSJH4D december 2010 – september 2020 BQ24133
PRODUCTION DATA
The output capacitor also should have enough ripple current rating to absorb output switching ripple current. The output capacitor RMS current ICOUT is given as:
The output capacitor voltage ripple can be calculated as follows:
At certain input/output voltages and switching frequencies, the voltage ripple can be reduced by increasing the output filter LC.
The BQ24133 has an internal loop compensator. To achieve good loop stability, the resonant frequency of the output inductor and output capacitor should be designed from 15 kHz to 25 kHz. The preferred ceramic capacitor has a 25-V or higher rating, X7R or X5R.