JAJSDT3A march 2017 – march 2023 BQ25601
PRODUCTION DATA
After the VBUS_GD bit is set and REGN LDO is powered, the device runs input source detection through the PSEL pin. The BQ25601 sets input current limit through PSEL pins.
After input source type detection is completed, an INT pulse is asserted to the host. in addition, the following registers and pin are changed:
The host can overwrite IINDPM register to change the input current limit if needed. The charger input current is always limited by the IINDPM register.