JAJSKU9B December 2022 – February 2024 BQ25628 , BQ25629
PRODUCTION DATA
In addition to boost OTG mode, the BQ25628 and BQ25629 provide bypass mode to directly connect the battery to PMID pin through BATFET and HSFET. The low impedance path in bypass mode achieves the highest efficiency when powering up external accessories, and maximizes the battery run time. During bypass OTG mode, the status register VBUS_STAT is set to 111.
Bypass OTG mode is entered when:
Any of the following conditions will exit from bypass OTG. Unless otherwise indicated, exit from bypass mode leads into battery-only mode by setting EN_OTG = EN_BYPASS_OTG = 0:
BQ25628 and BQ25629 can be configured to automatically transition between charging mode and bypass OTG mode by setting EN_CHG = 1, EN_OTG = 1 and EN_BYPASS_OTG = 1. When the adapter plugs in, and all conditions to start a new charge cycle are valid, the device automatically transitions to charging mode. If the adapter is removed and bypass enable conditions are valid, the device automatically transitions to bypass OTG mode to power the accessories connected to PMID.