JAJSEG2L October 2017 – March 2025 BQ2980 , BQ2982
PRODUCTION DATA
The device detects a UV fault when the battery voltage measured is below the UV threshold (VUVP). If this condition exists for longer than the UV delay (tUVP), the DSG output is driven to VFETOFF to turn off the DSG FET.
The device includes a UV_SHUT option which may be enabled during factory configuration. If this option is enabled, during the UV fault state the device goes into SHUTDOWN mode to preserve the battery. In SHUTDOWN mode, the BQ2980 will drive the CHG output to the PACK voltage, putting the device into ZVCHG mode (the BQ2982 does not enable this ZVCHG mode). That means, the CHG FET can be turned on if a charger is connected and both VDD and PACK meet the ZVCHG turn-on conditions (see Section 7.3.9 for more details). The PACK pin is internally pulled to VSS through RPACK-VSS. This is to determine if the charger is disconnected on the PACK+ terminal before shutting down the device. It is also to ensure the device does not falsely wake up from SHUTDOWN mode due to noise.
The UV status is released and the DSG output rises to HIGH, that is, VDSG = VDD × (1 + AFETON), if one of the following conditions occurs:
The device detects that the charger is attached if (VPACK – VBAT) > 700mV typical. To detect for load removal, the device checks if (VBAT – VPACK) < 400mV typical.
If the UV_SHUT option is disabled, during a UV fault DSG is turned off and the device does not go into SHUTDOWN. The power consumption is reduced to IFETOFF. The PACK pin is still internally pulled to VSS through RPACK-VSS. To recover UV with this option, one of the following conditions must occur: