JAJSK38 july 2021 BQ51013B-Q1
PRODUCTION DATA
Figure 10-4 shows wireless power start-up when the RX is placed on the TX. In this case, the BQ500212A is used as the transmitter. When the rectifier voltage stabilizes, the output is enabled and current is passed. In this case, the load is resistive generating 900 mA. The pulses on the RECT pin indicate communication packets being transferred from the RX to the TX.
Figure 10-5 shows a current transition. The plot shows a 1-A load removed then added again. Note the stability of VOUT.