JAJSRJ8B September 2019 – October 2023 BQ75614-Q1
PRODUCTION DATA
Ensure TSREF is enabled. To start the OT and UT protectors, host MCU sets OTUT_CTRL[OTUT_GO] = 1. When the device receives the GO command, it samples the following register settings and then starts the OTUT protectors accordingly. Any change of the settings below requires the MCU to send another GO command to implement the new settings.
The OTUT protectors can also operate in SLEEP mode. MCU first starts the protector in ACTIVE mode, then puts the device in SLEEP mode. The OTUT protectors will continue the operation until the MCU commands them to stop or if device shuts down.