JAJSRJ8B September 2019 – October 2023 BQ75614-Q1
PRODUCTION DATA
To start the OV and UV protectors, MCU sets OVUV_CTRL[OVUV_GO] = 1. When the device receives the GO command, it samples the following register settings and then starts the OVUV protectors accordingly. Any change of the settings below requires the MCU to resend another GO command to implement the new settings.
The OVUV protectors can also operate in SLEEP mode. MCU first starts the protector in ACTIVE mode, then puts the device in SLEEP mode. The OVUV protectors will continue the operation until the MCU commands to stop or if the device shuts down.