JAJSU42A April 2022 – April 2024 BQ76922
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Some device pins may not be needed in a particular application. Table 8-3 shows recommendations in which each should be terminated in this case.
Pin | Name | Recommendation |
---|---|---|
2–9 | VC0–VC5 | Cell inputs 1, 2, and 5 should always be connected to actual cells, with cells connected between VC1 and VC0, VC2 and VC1, and VC4A and VC5. VC0 should be connected through a resistor and capacitor on the pcb to pin 10 (VSS). Pins related to unused cells (which may be cell 3–cell 4, pins 3–6) can be connected to the cell stack to measure interconnect resistance or provide a Kelvin-connection to actual cells, in which case they should include a series resistor and parallel capacitor, in similar fashion to pins connected to actual cells (see Usage of VC Pins for Cells Versus Interconnect). Another option is to short unused VC pins directly to an adjacent VC pin. All VC pins should be connected to either an adjacent VC pin, an actual cell (through R and C) or stack interconnect resistance (through R and C). |
11–12 | SRP, SRN | If not used, these pins should be connected to pin 10 (VSS). |
13, 16, 19, 20 | TS1, ALERT, CFETOFF, DFETOFF | If not used, these pins can be left floating or connected to pin 10 (VSS). Any of these pins except for TS1 may be configured with the internal weak pulldown resistance enabled during operation, although this is not necessary. |
14 | TS2 | If the device is intended to enter SHUTDOWN mode, the TS2 pin should be left floating. If SHUTDOWN mode will not be used in the application, and the TS2 pin will not be used for a thermistor or ADCIN measurement, the TS2 pin can be left floating or connected to pin 10 (VSS). |
21 | RST_SHUT | If not used, this pin should be connected to pin 10 (VSS). |
22 | REG1 | If not used, this pin can be left floating or connected to pin 10 (VSS). |
23 | REGIN | If not used, this pin should be connected to pin 10 (VSS). |
24 | BREG | If this pin is not used and pin 23 (REGIN) is also not used, both pins should be connected to pin 10 (VSS). If this pin is not used but pin 23 is used (such as driven from an external source), then this pin should be connected to pin 23 (REGIN). |
25 | FUSE | If not used, this pin can be left floating or connected to pin 10 (VSS). |
26 | PDSG | If not used, this pin should be left floating. |
27 | PCHG | If not used, this pin should be left floating. |
28 | LD | If the DSG driver will not be used, this pin can be connected through a series resistor to the PACK+ connector, or can be connected to pin 10 (VSS). |
30 | DSG | If not used, this pin should be left floating. |
31 | CHG | If not used, this pin should be left floating. |
32 | CP1 | If not used, this pin should be connected to pin 1 (BAT). |