JAJSKT4J July 2021 – November 2023 BQ77216
PRODUCTION DATA
In the BQ77216 device, each cell input is monitored independently to determine if the input is connected to a cell or not by applying a 50-μA pull down current to ground that is activated for 128 μs every 128 ms. If the device detects that Vn < Vn–1 – VOW V, then a timer is activated. When the timer expires, the COUT and DOUT pins go from an inactive to active state. The timer is reset if the cell input rises above or below the recovery threshold (VOW + VOW_HYS).