JAJSN17 May 2022 CDCBT1001
PRODUCTION DATA
To ensure reliability of the device, follow the common printed-circuit board layout guidelines listed below:
Figure 10-1 shows an example layout for the DPW (X2SON-5) package. This example layout includes two 0402 (metric) capacitors, and uses the measurements listed in the package outline drawing appended to the end of this data sheet. A via of diameter 0.1 mm (3.973 mil) is placed directly in the center of the device. This via can be used to trace out the center pin connection through another board layer, or the via can be left out of the layout.