JAJSOF2 May 2022 DAC53202 , DAC63202
PRODUCTION DATA
The DACx3202 have four digital IO pins that include I2C, SPI, PMBus, and GPIO interfaces. These devices automatically detect I2C and SPI protocols at the first successful communication after power-on, and then connect to the detected interface. After an interface protocol is connected, any change in the protocol is ignored. The I2C interface uses the A0 pin to select from among four address options. The SPI interface is a 3-wire interface by default. No readback capability is available in this mode. The GPIO pin can be configured in the register map and then programmed in to the NVM as the SDO pin. The SPI readback mode is slower than the write mode. The programming interface pins are: