JAJS013I December 2000 – September 2020 DCP010505B , DCP010505DB , DCP010507DB , DCP010512B , DCP010512DB , DCP010515B , DCP010515DB , DCP011512DB , DCP011515DB , DCP012405B , DCP012415DB
PRODUCTION DATA
Multiple DCP01B isolated 1-W DC/DC converters can be connected in series to provide non-standard voltage rails. This configuration is possible by using the floating outputs provided by the galvanic isolation of the DCP01.
Connect the +VOUT from one DCP01B to the –VOUT of another (see Figure 7-6). If the SYNCIN pins are tied together, the self-synchronization feature of the DCP01B prevents beat frequencies on the voltage rails. The synchronization feature of the DCP01B allows easy series connection without external filtering, thus minimizing cost.
The outputs of a dual-output DCP01B can also be connected in series to provide two times the magnitude of +VOUT, as shown in Figure 7-7. For example, connect a dual-output, 15-V, DCP012415DB device to provide a 30-V rail.