JAJSMN8D December 2000 – August 2021 DCR021205 , DCR022405
PRODUCTION DATA
Two DCR02s can be used to create two +5-V output voltages, as shown in Figure 8-2. The two DCR02s are connected in self-synchronization, thus locking the oscillators of both devices to a single frequency. The ERROR and ENABLE facilities can be used in a similar configuration for a single DCR02. The filter capacitors connected to the VREC pins (CFILTER) must be kept separate from each other and connected in close proximity to the respective DCR02. If similar output voltages are being used, TI does not recommend that a single filter capacitor (with an increased capacitance) be used with both VREC pins connected together, because this could result in the overloading of one of the devices.