JAJSJ75C april 2020 – july 2023 DLP3010LC
PRODUCTION DATA
Operational DMD temperature and landed duty cycle interact to affect the usable life of the DMD. This interaction can be used to reduce the impact that an asymmetrical landed duty cycle has on the useable life of the DMD. Figure 6-1 describes this relationship. The importance of this curve is that:
In practice, this curve specifies the maximum operating DMD temperature that the DMD should be operated at for a give long-term average landed duty cycle.