JAJSFJ1 May 2018 DLPA4000
PRODUCTION DATA.
Be aware of the voltage coefficient of the decoupling capacitors. Physically undersized ceramic capacitors (with respect to the capacitance value to physical size ratio) experiences a large reduction in capacitance. Depending on the VIN voltage chosen and the voltage rating of the capacitors, physically undersized capacitors can experience up to a 90% reduction in capacitance, leading to insufficient decoupling.
Choose decoupling capacitors (C17 and C119) with a value of 0.1 µF and a size of 0402. Place the decoupling capacitors as close as possible to the power block VIN pins. Even an increased distance as small as 1 mm in compared to the reference design can cause a large increase in voltage ringing amplitude. Because the parasitic inductance of the route combined with the effective inductance of the capacitor affects the switching node, select capacitors with a higher SRF rating. Place the VIN decoupling capacitors on the top layer very close to the power blocks to minimize parasitic inductance. Place the 10-µF decoupling capacitors (C18, C114, C115, C116, C117, and C118) near the power blocks, They do not need to be as close as the 0.1-µF capacitors.