JAJSGN4F August 2012 – February 2019 DLPC410
PRODUCTION DATA.
NS_FLIP allows the user to specify the loading direction of rows in the DMD when used with ROWMD = “01”. This control has no effect if ROWMD = “10”.
Row Addressing and Table 12 describe the effect of N/S flip. If NS_FLIP is set, this does not reverse the direction of Mirror Clocking Pulse groups (blocks). For example, the normal case is to Mirror Clocking Pulse blocks 0 – 15 in order. When NS_FLIP is set, the order of block Mirror Clocking Pulses must be reversed to 15 – 0.
The NS_FLIP signal should be kept low during initialization to ensure proper setup of the system.