JAJSGN4F August 2012 – February 2019 DLPC410
PRODUCTION DATA.
The last portion of the initialization process involves a series of commands sent from the DLPC410 to the DMD. During this step, check the output of the DLPA200(s). One should expect to see several Mirror Clocking Pulse waveforms indicating the DLPA200(s) is (are) initialized correctly.
This will complete the initialization process. When the initialization process starts, the INIT_ACTIVE ouput signal (pin AA18) will assert (go high) indicating that the initialization sequence is in process. At the end of the initialization sequence, if the initialization is successful, the INIT_ACTIVE ouput signal (pin AA18) will deassert (go low) indicating that the initialization process is complete.
NOTE
Initialization complete indicates that the initialization sequence of the DLPC410 has completed, but does not ensure that each step was completed correctly, only that it finished. For example the initialization of a DLPA200 may complete, but if the voltages set are incorrect further investigation is needed to uncover the reason.