JAJSTJ2 June 2024 DRV2911-Q1
PRODUCTION DATA
The device is fully protected against any cross-conduction of MOSFETs - during the switching of high-side and low-side MOSFETs, DRV2911-Q1 avoids shoot-through events by inserting a dead time (tdead). This is implemented by sensing the gate-source voltage (VGS) of the high-side and low-side MOSFETs and ensuring that the VGS of the high-side MOSFET has reached below turn-off levels before switching on the low-side MOSFET of the same half-bridge (or vice-versa) as shown in Figure 6-15 and Figure 6-16.