JAJSVQ6 November 2024 DRV81004-Q1
ADVANCE INFORMATION
DRV81004-Q1 has two input pins. Each input pin is connected by default to one channel (IN0 to channel 2, IN1 to channel 3). Input Mapping Registers MAP0 and MAP1 can be programmed to connect additional or different channels to each input pin, as shown in Figure 6-2. The signals driving the channels are an OR combination between EN register status, IN0 and IN1 (according to Input Mapping registers status).
The logic level of the input pins can be monitored via the Input Status Monitor Register (INST). The Input Status Monitor is operational also when DRV81004-Q1 is in Limp Home mode. If one of the Input pins is set to logic high and the nSLEEP pin is set to logic low, the device switches into Limp Home mode and activates the channel mapped by default to the input pins.