JAJSVQ9 September 2024 DRV81620-Q1
ADVANCE INFORMATION
The device supports multiple protection features, discussed in detail in the subsequent sections. The SPI interface provides diagnosis information about the device and the load status. Each channel diagnosis information is independent from other channels. An error condition on one channel has no influence on the diagnostic of other channels in the device (unless configured to work in parallel, see Section 7.3.3.5 for more details).