SLVSGC3 May 2020 DRV8210P
PRODUCTION DATA
An analog current limit circuit on each MOSFET limits the peak current out of the device even in hard short circuit events. If the output current exceeds the overcurrent threshold, IOCP, for longer than the overcurrent deglitch time, tOCP, all MOSFETs in the H-bridge will be disabled. After tRETRY, the MOSFETs are re-enabled according to the state of the IN1 and IN2 pins. If the overcurrent condition is still present, the cycle repeats; otherwise normal device operation resumes.