JAJSU39 April 2024 DRV8235
PRODUCTION DATA
The voltage on the VREF pin selects ITRIP threshold which sets the current level for stall detection and current regulation. This threshold should be chosen such that ITRIP is less than the stall current of the motor when current regulation is not used. It should also be set low enough to account for variation in the stall current due to changes in the motor supply voltage, VVM, and temperature.